This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28070: Multiplier settings at DC input

Part Number: UCC28070
Hi,
The other day, when using the UCC28070 with DC input, we received a response
that it is recommended to drop the VINAC pin low at 3.4 mV/us or less.
If I drop it low at 3.4mV or higher and let it continue to row for 1ms, will the multiplier level be set correctly?
Also, is there something going on?
 
Best regards,
  • Hi User,

    the 3.4mV/uS is suggested by designer of this controller mostly depends the sampling precise.

    from application view, I would suggest we can follow the suggestion, much higher or much lower than this value should cause a wrong sampling of Vinac Zero crossing signal.

    hope this helps you.