This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25221: To replace TPS2551 with ILIM short to In

Part Number: TPS25221
Other Parts Discussed in Thread: TPS2553,

Dears

My customer is using the TPS2553 with ILIM short to In, in this case, the current limited point is 50 -100mA. But customer need a higher current version which can make drop in replacement . 

we have found that the TPS25221 is P2P with TPS2553, and TPS25221 have higher current limit range with same Rilim. but in the datasheet, there do not mentioned that, when ILIM short to In, the output current limited range. So we are wondering:

1. if the TPS25221 can support the  ILIM short to In?

2. if point one is ok, how about the current limited range when ILIM short to In?

Thanks

Jun Shen