This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS745-Q1: Package of TPS745-Q1

Part Number: TPS745-Q1

Dear Team,

Our customer have a question as below

Package of  TPS74510PQWDRBRQ1 is VSON  DRB (8 pins), right?

Many Thanks,

Jimmy

  • Hi Jimmy,

    This portion of our datasheet pulls automatically. Yes DRB is VSON package. In this case we refer to it as SON per standard definition - "Small Outline No Lead, also referred as DFN = Dual Flatpack No Lead". There are some few more edits that need to be on the datasheet and we'll make sure to update this accordingly.

    regards,

    Wilson