In my design, the input power cycles on and off.
While the device works as expected, we have seen a skipped cycles. That's the output is off.

In this scope picture, the green line is the input, Blue is the output and yellow is the PG.
The circuit design is as follow:
The input voltage is 12VDC.
Current consumption in less than 1A
Appreciate your input/help.