Other Parts Discussed in Thread: BQ76952, , BQ76920, BQ76930, BQ76940, BQ34110, BQ34Z100-G1
1) Is BQ78350 feasible for BQ76952?
2) Can I use BQ78350 for 24S 72V battery?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gururaj,
The BQ78350 can only work with the BQ76920 / BQ76930 / BQ76940 family of battery monitors. It will not work with the BQ76952.
I also do not recommend using the BQ78350 for a 24S battery. It is designed to work with only one BQ769x0 device, so 15S is the maximum it can comprehend. I recommend the BQ34110 or BQ34Z100-G1 for a 24S battery. You can look at TI Reference Design TIDA-001030 for an example using the BQ34Z100-G1 with a battery monitor.
Best regards,
Matt