This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5170: Disable diode emulation mode

Part Number: LM5170

Hello support team,

Can LM5170 disable diode emulation mode? If yes, please explain how to disable it.

Thanks,

Koji Ikeda

  • Hello Ikeda-san,

    The LM5170's diode emulation is always activated.  In order to disable it, you need to introduce a dc bias signal to the current sense. Could you tell which mode do  you need to "disable" the DEM,  in buck, or boost, or both? 

    Thanks,

    Youhao

  • Yuohao-san,

    Thank you for your support.

    Customer has concern in load transient at Buck CV mode. If diode emulation might have pulse skipping at very light load, this might cause poor load response. Do you have any way to improve it?

    Thanks,

    Koji Ikeda

  • Hi Ikeda-san,

    Yes there is a way to work around.  That is to introduce a offset voltage to the current sense signal.   A simple way is to place a few kOhm resistor from CSB pin to GND, which forms a resistor divider with the CSB pin series resistor (1~2 Ohm) and introduces a dc bias by slightly pulling down the CSB pin voltage. 

    Hope this clarifies.

    Thanks,

    Youhao