Hi
I am using a 3 x TPS54160 devices to get a sequenced 3V3, 1V8 and 1V2 from a 24V input. According to the datasheet placing a 270k resistor on the RT/CLK input should result in a switching frequency of about 444kHz on the 1V2 PSU. However, it appears that, the switching frequency defaults to the minimum of 300kHz and in some instances the device starts skipping.
This 1V2 PSU is used to power the core of a DSP and this skipping (or Ecomode) seems to result in the DSP core not starting up properly. My calculations based on the data in the datasheet suggest that the 444KHz is well below the curve of the skip and shift frequency.
Any ideas as to why this frequency would not be 444KHz as expected and how to get rid of the skipping?
Thanks
Morag