Hi
I performed a discharge-charge-discharge cycle in order to create a AUX file for LifePO4 Pack and BQ78PL116,
the result was:
"Prereading data
........................................................................................................................
.........................
bad data in line 14564 skipped
Preread is Complete
Final Discharge from T = 443.870 to 567.512 shows capacity of 10209 mA
Current measured for first discharge was = 4951 mA for an error of -0.980 %
Compiling profile of data file
Processing cycle : 1
Initial Discharge Complete
Initial Discharge Complete
Charge Complete
Second Discharge Started
Second Discharge Complete
Processing cycle : 2
Initial Discharge Complete
There were one or more problems:
impedances Could not calculate 120 impedances
====================================
There was a problem found:
AuxGen could not calculate all impedance values needed
Please contact TI support for assistance
This is a fatal error and no .aux file will be generated"
can anyone point out the the problem that the program was not able to calculate the impedances? (Ra)
please I'm realy stuck on this
thanks