This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53353: IVFB conditions

Part Number: TPS53353

Hi,

Why is the VVFB value listed in the IVFB conditions of the data sheet 0.63V?

Best Regards,

Nishie

  • Hi Nishie,

    The TPS53353 has an internal reference voltage of 0.6V, so the value of VVFB will be 0.6V in a closed-loop configuration. The value of 0.63V listed in the IVFB conditions was measured forcing the feedback voltage to 0.63V in an open-loop test environment and then measuring the resulting current. That is why the 0.63V value is listed in the IVFB section. 

    Regards,

    Alec Biesterfeld