This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54331: very important noise at the output of the buck

Part Number: TPS54331

Hello,

I use a TPS54331D but I have noise like in the following photo,

scope

here is my montage.

Does anyone have any idea of my problem?
I want an input voltage of 7V and 18V with an output voltage of 3.3V and 3A.

the noise rises to 6V and repeats about every 2 ms. The rest of the time, I have 3.3V output