Will the VIN and VOUT connections turn off completely when the device goes into sleep mode(VIN_LOWV < VIN < VOUT + VSLEEPZ )?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Will the VIN and VOUT connections turn off completely when the device goes into sleep mode(VIN_LOWV < VIN < VOUT + VSLEEPZ )?
Hello Noriaki,
In sleep mode there is still some internal circuity powered on. In my testing with Vin 3.4V and VOUT 3.6V, the current consumption from VIN current will be around ISTANDBY_IN (~200uA). The battery Iq is around 4uA in this mode.
For lowest battery Iq you should also disable charge, pull /CE high (~350nA).
Nick
Thank you for your answer.
I have additional questions.
Is there never a current flowing from VOUT to VIN?
Hello,
The bq25171-q1 will prevent reverse current from from VOUT to VIN.
Best regards,
Nick