This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28951-Q1: EV Battery charger 40-57 V 40A

Part Number: UCC28951-Q1
Other Parts Discussed in Thread: UCC28951, UCC28950

Hello sir,

We are trying to design a battery charger of output voltage  range 40 to 57 V  with 40 A as CC current .Our operating switching  frequency is 50kHz. We have selected PSFB as our second stage converter for which we are using UCC28951 as our controller IC . We want to provide Different adaptive delays to Leading leg  Switches (A and B) and lagging leg switches (C and D) .We have decided to short the CS pin and ADEL pin as  well as ADELEF Pin  so that we can get maximum adaptive delay based on CS pin Voltage.  Will it work if we do so? Also I have the following questions -

  1. For adaptive delays based on CS pin voltage do we need to connect RDELAB and RDELCD and RDELEF  as well.
  2. If we short the CS pin with ADEL what will be the CS pin voltage at the time of ZVS ??
  3. How to select the value of RA and RAEF  if RAHI and RAEFHI is Zero .

Regards