I have a project with 3740 ~ 5060VDC input, 24V output, and 150W power. Is there a suitable solution to recommend?
Can I use two high-voltage MOS or IGBTs in series to replace the MOS in the low-voltage DC/DC solution. Such as IXTT02N450HV, IXTX1R4N450HV, IXYT30N450HV.