Other Parts Discussed in Thread: LP8864-Q1
Hi,
I have a questions.
1. The current values of LP8864S-Q1 and LP8864-Q1 are different. Can the peripheral circuits and software be used in the same way?
2.Can LP8864S-Q1 flow 200mA (ILED) to each channel? P21 of the data sheet says "For high accuracy of LED current, the ILED current is recommended to set in range from 30 mA to 200 mA."
Is the recognition that ILED = 150mA wrong?
Best Regards,
Nishie