This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25066I: disablling UVLO and OVLO?

Expert 6470 points
Part Number: LM25066I


Hi there,

is it possible to turn off the UVLO and OVLO, by connecting them respectively with VDD and GND (without additional resistors)?

Thanks!

  • Hi Bart,

    Thanks for reaching out to us. UVLO/EN can be connected directly to VDD if input voltage is above 3.3 V and OVLO directly to GND to disable under-voltage and over-voltage functionalities respectively. For input voltages 3.3 V and below, VDD and UVLO/EN should be tied directly to VIN to avoid the dropout of the sub-regulator. External pull-up or pull-down resistors are not required.