Part Number: UCC28782
Other Parts Discussed in Thread: UCC28780,
Hi,
I would like to know what are the mean features of the UCC28782 in comparison with the UCC28780. It appears like they have similar controle modes of the Active Clamp Flyback and similar protections.
I'm using the UCC28780 for a low power supply aerospace application :
Vin = 115V ; 400Hz
Vout = 30V ; 30W
Knowing that my main interests are to increase the efficiency of my power supply while successfully passing DO160 EMI standards, is it more advantageous for my application to switch to UCC28782 ?
Thank you in advance for your answer.