This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Monitoring and Protection without balancing

Part Number: BQ76952

Can this IC be used without the balancing feature? We plan to use it for a 16s system for monitoring and protection only. The balancing will be done elsewhere which is why I would like this IC to ignore the balancing features.

Thanks!