This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24196: Battery REG08[5:4]

Part Number: BQ24196


Hi,

BQ24196 has connected to my board I2C line and my board is required to run 3.7V that's y I choose 3.7V battery. Here the condition is while board running time if any main power fluctuation gets it should be switchover from main to the battery like as UPS.

while running time if any power interrupts I am not running the battery for more than 10 min. the 10th minute I am disabling the BATFET (because of to avoid the battery drain).

I observed REG08[5:4]  status some times 00 showing and some times 11 is showing.

00 - Not Charging

11 - Charge Termination Done.

[71, 29, 0, 17, 178, 136, 3, 11, 132, 0]  // this is the  battery all register values. it is in Decimal format

[71, 29, 0, 17, 178, 136, 3, 11, 180, 0] // decimal format

here decimal 132 is for REG08

180 also REG08