Other Parts Discussed in Thread: UCC38C43, UC3842
I implement UC2823A on a prototype and starting the moke up.
As I want to use it in voltage mode, I connect RAMP with CT.
I get an output signal at the expected frequency (200kHz), but I'm not able to get small duty cycle:
If I drive EAOUT voltage from 4V down to 2.5V, I control the duty cycle from 99% to 40%. But if I continue to decrease EAOUT voltage, I loose the output signal: I'm not able to have duty cycle less than 2us
If I increase the value of CT capacitor, the frequency of course decrease, but I'm still limited at 2us.
Why is it not possible to get small duty cycle with this component, in voltage mode?

During the test I already modified several things in this schematic:
- Vc connected to +12VD
- Q220 short circuited to connect R223 to 0VP
- C221 and R221 disconnected
Thanks for your support