Hi
From 18V to 28V, short circuit protection is not garantee for the over all temperature range.
Is it possible to estimate the max Vbb value for the temperature range from -20°C to 50°C?
Could the component handle short circuit with Vbb=24V and ta=50°C?
BR