Hi
Use EVM of LM73100 to make Oring circuit, when one of them has no input,
The LM73100 without electricity has leakage at the DV/DT pin, which is about 16.xV When the input voltage is 19V
1. Will it cause damage to the IC?
2. Why is there will be leakage design, this is normal?