Part Number: BQ28Z610-R1
Hello!
From section 7.26 of the BQ28z610-R1 datasheet, it states there is a 3.3k pull down on I2C. Can you elaborate on this PD? Could the voltage divide from the external I2C pullup and not be in compliance to voltage level requirements?

Additionally, for a single cell application, what are the recommended Vc1 and Vc2 connections and R/C values? Section 9. 2 typical application circuit shows 2 cell, and it appears that the 100ohm, 5ohm, and 1uF may need adjustment for single cell.
Thanks!