I have 3 TPS76333 ,and on the outputs i measure 3,8 V not 3,3? is it ok? how could this happen? or am i doing something wrong??? what should I do to have 3,3V not 3,8?
thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have 3 TPS76333 ,and on the outputs i measure 3,8 V not 3,3? is it ok? how could this happen? or am i doing something wrong??? what should I do to have 3,3V not 3,8?
thank you!
Does the output voltage regulate to 3.8V regardless of input voltage and load current (up to 150mA). Did you check the package top marking to make sure you have the correct ICs? 3.3V option should read PBEI. 3.8V option reads PBFI. If that is not the problem, can you provide a schematic and input voltage?
Hello Gyorgy,
No this is not ok. Have you looked at the output on an oscilloscope to see if the output is oscillating. Please make sure that the output capacitor meets the requirements found in the Apps Info (and Figures 16-19) of t he data sheet.
Bill
The marking should have four letters starting with P. If not, then you may not have the correct IC.