Adding An External Symbol To PSpiceTI library
I am using PSpice for TI, and I am trying to add a model of component ISL75052 to the PSPice libray, so that I can run a simulation on the part.
I got a model file(isl75052eth.lib) from the manufacturer of the part, but I cannot figure out how to add the part model to the PSpice tool and create a symbol automaticallly for the part.
Has anyone out there ever have to add an external model&symbol to the PSpiceTI library and run a simulation on the part?
I was reading through PSpice users guide and it talks about using the symbol editor. However, I created a new schematic project and could not see how to start-up the symbol editor. It does not appear as if I have access to the symbol editor.