Other Parts Discussed in Thread: UCC28051, UCC28501, PMP30446, UCC23313-Q1, UC3823
Hi Team,
We would like to ask your help regarding the customer's inquiry below.
I am looking for a controller for switching a buck converter (or a syncron converter). The input voltage will be 390V to 410V and the output voltage should be 380V. Therefore i will need a driver and an isolation transformer for the gates. But first of all i need a controller. Therefore I am looking for your help to find the right one.

The gates of T1 (and T2) will be connected via an isolated driver to the controller i am looking for.
According to the customer, the supply to the controller could be 3.3V,12V or 24V.
Thank you for your support!
Regards,
Danilo