This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS565201: Cout = 150uF

Part Number: TPS565201
Other Parts Discussed in Thread: TINA-TI

Hi,

I'm using the TPS565201 and need to have a total of 150uF of Cout (15 x 10uF MLCC).  My output voltage is 5V and I'm using L=10uH.  The datasheet says max Cout is 68uF.  I have seen other issues on the E2E regarding this part saying to reduce the value of L to keep the "loop stable".  Question is how to calculate the value of L for a given Cout?.

thanks