This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB-PD-CHG-EVM-01: How to flash: USB-PD-CHG-EVM-01?

Part Number: USB-PD-CHG-EVM-01
Other Parts Discussed in Thread: USB2ANY, TPS25750

Hi

I am trying to flash USB-PD-CHG-EVM-01 using this USB to I2C converter. But the hardware connection between the GUI is not connecting.

Also I tried using a USB type C cable, here also the GUI is not detecting the hardware.

During the above two state battery is connected to the J2 or battery input connector of USB-PD-CHG-EVM-01.

Please clarify the following.

  1. Is that possible to flash the EEPROM in USB-PD-CHG-EVM-01 the USB to I2C converter
  2. Can I directly flash the EVK using the USB type C cable?
  3. Is there any other flashing options in USB-PD-CHG-EVM-01 than USB2ANY and Aardvark, since both are very costly.