This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL494: Oscillator frequency

Genius 17555 points
Part Number: TL494


Hello,

 

My customer has a question for oscillator frequency of TL494.

 

They are using 12.2Kohm+-1% for RT and 0.1uF+-10% for CT and the actual oscillator frequency is about 1.15KHz.

But from the below figure on the datasheet, the oscillator frequency with12.2KOhm and 0.1uF should be around 0.9~1KHz.

So they feel actual frequency, 1.15KHz, is a littlie bit different from the figure, 0.9~1KHz.

Is this 1.15KHz reasonable value? Or anything wrong?

 

Regards,

Oba

  • Hi Oba,

    The graph you are showing is on a log (y-axis), log (x-axis) and gives a fairly "linear" approximation but the actual F vs RT, CT relationships are non-linear. I would say that if the target frequency from the graph is 900 Hz<F< 1kHz and the actual measured frequency is 1.15 kHz, this is within 15% which is very good for a first pass. The graph gets the design in the "ballpark", the final target value can be adjusted on the bench. Also, when you are targeting frequencies at the extremes of the graph (such as 900 Hz-1 kHz), the degree of error is higher compared to midband frequency targets such as 10 kHz-100 kHz. 15% error near 1 kHz is excellent!

    Regards,

    Steve M