Other Parts Discussed in Thread: UCC28911, , TPS63802
Greetings,
We are looking to power a device with GSM modem which takes 2A peak current for 0.6 ms every 4.6 ms whenever it is communicating (2-3s). The two power sources that we are considering for this application are a buck DC-DC converter such as UCC28911 (70V Vin and 5V out with 0.5A max) and a Li-Ion battery (4.2-3.2V, 3.8V nominal). These two sources are to be selected automatically with DC-DC as higher priority. The output of the PPM is given to a buck-boost TPS63802 to give a stable 4V for GSM module. This is as shown in block diagram below where we feel BQ24079 is appropriate as the power path manager with its supplement mode, configuring the input limit as 0.5A.
Can BQ24079 go to supplement mode for a instantaneous spike of 2A for 0.6 ms? Do you see any other issue with this setup?
Thanks, Prithvi