Hello,
On the device, we have the exact chem ID (EVE LF105 number 4118), and the learning cycle went well.
At the end of discharge, after entering the relax mode. DOD0 updates from 0 to 16145mAh.
This value is to High. Our battery is a 105Ah and Current is scaled 1:10, I should expect something close to 10500, Right?
If DOD0 measurement is wrong at End of charge, does It mean there is a mistake in the Chemistry ID 4118?
I assume you need a lof of the discharge and a .gg file to help me.
In the log file, the sample 9878 shows the updated value of dod0.
Thank you verry much!