This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51003: without using the communication features

Part Number: BQ51003


Hello Guys,

Good day.

Our customer is wondering if  BQ51003 still is functional without using the communication features on it?

Also, what compatible transmitters work best with it currently and do these transmitters function without the communication features?

Thanks and regards,

Art

  • Hello Art

    Sorry, but cannot run the unit without communications feature.  This is part of the Qi standard and both unit will shutdown in a no communications situations.

    The BQ51003 will work with any Qi transmitter.  

    I like to recommend the TYLT Vu and TYLT Vu Solo