Other Parts Discussed in Thread: BQSTUDIO
I'm trying to use BQ27Z561 in my real system. I performed a successful learning cycle with my single-cell battery pack, the EVM and BqStudio and gotten a golden image.
[Q-1] As a trial I would like to upload this golden image into another EVK I have, which has the same battery and did not perform a learning cycle, using BqStudio.
How do I do this?
[Q-2] Let's assume I managed to use slua810 to load the golden image into the FG on my system without using BqStudio.
Is there anything I need to change in the FG configuration after loading the golden image (e.g., empty voltage, spare capacity, etc.)
and how would I know what to change them to?
Are there parameters that are usually/recommended to change on the real system?
[Q-3] Do I need to perform (periodic?) calibration on my system?
Is there a document describing which calibrations to perform, how to, and when?
Thanks,
Ofer