This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25910: Ic-load definition

Part Number: TPS25910

Hello Experts,

I would like to know definition of Ic-load in equation 11 of the datasheet. Ic-load is maximum load current, correct? If no, please correct me.
[condition]
Vin: 5V
Ic-load: 3A
C-load: 47uFx2

delta T= (47u*2*5)/3 = 156.667u
Cext = 11u * (156.667u /5) - 200p = 144.6674pF <= Is the calculation correct? If so, can I use 100pF for Cext?

Best Regards,
Fujiwara