SPNA176A–February 2014...Figure 1. Example TPS65381 With Texas Instruments TMS570/RM4x
shows the nERROR siignal from the HERC going to he WDI/ERROR pin of the TPS65381.
Is this ok if using TRIGGER mode?....
I have been using the TRIGGER mode of the TPS65381 (not the Q&A mode) and driving the ERROR,WDI pin of the TPS65381 with a GPIO pin of a few different Microprocessors, ( basically setting the uP to interrupt on a specifiic time and then synching the uP to the TPS65381)...that works fine...
the nERROR pin on the Herc appears to be a pin that will "flagg error, i.e. go LOW), if something internal in the Herc goes wrong (i.e. voltage level off, etc etc)....
just want to make sure I can use that nERROR pin as a WD pulse to the TPS65381. (i.e. set a timer interrupt in the Herc and then pulse that nERROR pin with a pulse that meets the Window/1 WINDOW 2 timing of the TPS65381)..
thank you or any insight!....
cheers
jyoung@dcscorp.com