Hi,
We are designing an LM25117 circuit with constant current control, and we have had some failures (4/10 boards have failed) due to some component shorting or burning up. I have attached the circuit implementation for review to see if we can get some feedback on it. The parts that fail have a black square around them (Q1, Q2, C19, C20, C21, C22). We have added significant heat-sinking on the L1 inductor for the current board revision, and the inductor temperature saturates at 95 F - 100 F. The inductor is placed close to the Q1/Q2 copper pad (linear distance to Q1is 12 mm, linear distance to Q2 is 7 mm). We have been researching application best practices on the LM25117, and maybe we are missing some protection feature or circuit on the MOSFETs and output.
Q1/Q2 P/N: BSC066N06NS
C19-C22 all rated at 50V. Output nominal max is 24V.