Other Parts Discussed in Thread: BQSTUDIO
Hello,
We have designed a portable device with BQ25890H to charge a Lithium battery.
We must customize the JEITA Profile T5 temperature to 45°C.
Because our new battery cells accept only a charge at maximum 45°C.
Is it possible to do this?
Or if it is not, is it possible to change some components values of the BQ25890H to stop the charge at 45°C?
If we change the value of RT1 and RT2 to define a maximum at 45°C with R_HOT = 4.92KOhms.
Do you think it is possible?
But in this case, the COOL and WARM threshold will be not at 10°C and 40°C. Is it possible to adjust these parameters?
Thank you in advance for your help.