This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63802: Problem for PG output function

Guru 19685 points

Part Number: TPS63802

When TPS63802 circuit startup, power good operation is following with Vout startup.

I hope to move power good start to switch high when Vout reach 95%. (The same PG behavior on datasheet P26: Figure 10-30 and 10-31)

If there any adjusting point, please let me know.

TPS63802 circuit condition is below;

・Vin: about 4.2V (battery), Vout: 5V, Iout: 1.8A, L: 2.2μH

・PG output is 100kΩ pullup to Vout

・EN pin is controlled by external ON/OFF signal (not connected to Vin)

・tss: about 4sec, Cout: 47μH ×4 for decrease ripple 

・Waveform is below; Yellow: EN, Green: Vout, Blue: PG, Red: Vin

 ※Vout startup line is overlapping with PG 

・Waveform for focus PG and Vout is below; Yellow: Vout, Green: PG

Best regards,

Satoshi