How to calculate the current consumption (Icc) of BQ24230.
IN pin: Nothing is connected.
BAT pin: 3.7V.
OUT pin: A load carrying 100uA of current is connected.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Welcome to E2E!
You can use the IBAT(PDWN) value as your baseline and then add the current that is being drawn by your load. At max, you'll see IBAT(PDWN) is 6.5uA and so you should see 106uA of current consumption when in a battery only powered state for your scenario.
Best Regards,
Anthony Pham