This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ3050: config parameter read

Part Number: BQ3050
Other Parts Discussed in Thread: EV2400, BQSTUDIO

Hi Team

It is first time customer uses BQ3050, and wants to read the config parameters of BQ3050, such as the overvoltage protection point, can it be read through the MCU software, or how to realize through the EV2400?  By the way, could you help on providing BQ3050 BQZ file also?

Best Regards

Gene

  • Hi Gene,

    They can use an EV2300 or EV2400 to read config parameters. There is no BQZ file for this device so they will need to use bq3050EVSW instead of bqStudio. They can download the EVSW on the BQ3050 product page.

    Best,

    Jessica