Other Parts Discussed in Thread: LMZM33602EVM, LMZM33602
Hello team,
I received a question from my customer about thermal shutdown of TPS7A9201DSK. I would appreciate it if you could provide us some advice about the following 3 questions.
◆ Environment
Assumes input 3.3V/output 1.2V, load current up to 1.561A or less.
◆ Questions
(1) When using the maximum current value in the above situation, it is likely that the junction/case temperature would exceed 200°C at an ambient temperature of 25°C.
The data sheet confirms that ThermalShutdown will function at approximately Typ160°C before reaching this temperature.
When the temperature exceeded shutdown temperature threshold, does this IC turn off and drops the output voltage (output Enable off?) immediately? Or does it have some delay time?
(2) Are there any pin compatible device for TPS7A9201DSK that the junction temperature is within the operating temperature range under the above conditions
(3) If there are no devices that meets question 2, they would like to place the Buck Converter EVM, which has an input voltage (DC) of +24V, an output voltage of 1.8V, and a maximum load current of 1.561A, in front of the TPS7A9201DSK.
The current candidate is LMZM33602EVM. Are there any other EVM candidates with a lower price and a smaller area?
Best Regards,
Ryotaro Fukui