Other Parts Discussed in Thread: UCC27423-EP,
I am driving a gate drive transformer (240uH) with the UCC27423-EP, UCC27424-EP gate driver IC outputs. Do the integral body diodes of the MOSFET outputs protect the outputs of the driver IC when switching inductive loads? The data sheet is nor clear. I actually make a H-bridge with 2 UCC27423-EP, UCC27424-EP outputs. Like a DC motor driver. This way I can generate positive or negative output voltage from a single bias supply. Do I have to use external clamp diodes from the driver output to rail and ground to protect from Ldi/dt? Please advise.
Thank you.
Jim