This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63810: Will the converter work without connecting the I2C

Part Number: TPS63810
Other Parts Discussed in Thread: TPS63805

Hello,

I need to use a buck boost to provide a stable 3.3V and found the TPS63810.

I saw in the datasheet that the output voltage can be selected via VSEL and also via I2C.

If I only need the 3.3V output, will it work connecting VSEL to GND and leaving the I2C pins disconnected?