Part Number: REF200
In datasheet, I am seeing -25 and 85 as minimum and maximum operating temperature but nothing mentioned about junction temperature range. Also I can see current variation with temp graph andtemperature specify from -50 to 125 deg C. So whether device can operate from -40degc to 125 deg C junction temperature?
Also no where mentioned about junction to case temp or ambient temp in datasheet, how to calculate that. Whether part is qualified for Industrial grade?
My requirement is to work from -40 deg C to 95 deg C with 12V supply and 0.1mA both channel use. Whether this part can meet this requirement?