Hi Team,
In the datasheet section called Battery Under-Voltage Lockout Comparator, it seems to say that the battery FET (Q5, driven by the CMC's BATDRV pin), will be driven open if VBAT falls below 2.4V (typical). This is fine for a single cell. But for 4 cells, we need the FET to open if VBat falls below 2.4V * 4 = 9.6V. We are using 4 QB18650 3.7V 3000mA batteries connected in series and a battery must not discharge below 3V
We don't see anything in the datasheet that explains if that voltage is multiplied by the number of cells indicated by the cell configuration. My question is what is the VBAT_UVLO for 4 cells?
Thank you,
-Mark