Dear team
There is a good news that we design in LMR33630-Q1 in customer's new project.
Could you help to review the schematic(U28 and U26)?
spec of U28 : Vin =9V~16V, Vo=5V, Io=2A
spec of U28 : Vin =5V, Vo=3.3V, Io=2A
Many thanks
Denny
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team
There is a good news that we design in LMR33630-Q1 in customer's new project.
Could you help to review the schematic(U28 and U26)?
spec of U28 : Vin =9V~16V, Vo=5V, Io=2A
spec of U28 : Vin =5V, Vo=3.3V, Io=2A
Many thanks
Denny
Hello Denny,
Both Schematics look good. I believe customer followed Table 8-2 in the datasheet (which is good). In regards to 3v3 output schematic, L5 is 1.5uH, which should be okay. Table 8-2 does recommend a higher value of 2.2uH, so perhaps customer made a typo (if they were following table 8-2). Regardless, 1.5uH should be okay. Just wanted to point that out.
Kind regards,
Alejandro
Hi Denny,
For U28 section:
1. Input cap 35V--50V rating, output cap 16V rating
2. Add 0ohm in series C211
3. Reduce R446+R133 to 10K~22K range
4. C368 is DNP
For U26 section:
1. Input cap >16V rating, output cap 10V rating
2. Add 0ohm in series C223
B R
Andy