Hi,
We are doing a learning cycle process for our fuel gauge BQ34Z100-G1.
Our battery specifications are
Name: Exide EP42 - 12
Voltage: 12V
Capacity: 42Ah
We have figured out CHED-ID for our battery profile as 801.
In the attempt to learning the cycle for this fuel gauge and battery combination, we failed multiple times as our update status is not changing to 0x05. Before attempting a new learning cycle, we thought that we should reverify our data flash configurations.
As mentioned in the application note of the learning cycle, for a successful learning cycle we need to configure Design Capacity, Design Energy, Quit Current, Taper Current, and Termination Voltage.
But as we go through multiple posts on the TI forum regarding the failure of the learning cycle we came to know that there are many such parameters that need to be configured and their values can lead to failure in the learning cycle. We don't have clarity about many parameters.
The following parameters are discussed frequently in the TI forum and we are unsure as do we need to change these parameters for a successful learning cycle or go with the default value. Because these parameters are nowhere mentioned in the application note.
If someone can spread some light on the below parameters then it would be a big help.
1. Taper Current (After searching the forum we found that it should be between C/100 to C/10. For our case we have figured out it as (42000 / (ScaleFactor = 10)) / 20 = 210 mA )
2. Min Taper Current
3. Cell Taper Voltage
4. FC Set % (default is 100% but in some cases, they set it as -1. )
5. FC Clear %
6. SOC1 set/clear threshold
7. SOCF set/clear threshold
7. Load Select (default is 1 but how to select this value. Does this have any relation with learning cycle success ?)
8. Load Mode (0: constant current, 1: constant voltage)
We have gone through its description in this note: slua664 but it is still unclear that do we need to change this parameter or go with the default values to achieve a successful learning cycle.
Our design capacity is 42000 mAh which is scaled down to 4200 by a scale factor of 10. Same way design energy = 8400.