I am currently evaluating this chip for use with a 6V 10W solar panel, charging a 2S Lipo setup. Ultimately it will be interfaced with a MCU and i2C functionality to be fully utilised, particularly the MPPT feature.
However as a fallback I want the device to be able to operate standalone. I am using the EVM kit and 2400 interface to see the register settings etc.
I have however noticed, a particular situation, similar to a previous poster regarding slowly rising input voltages, that when the panel is covered and slowly uncovered, emulating a day night cycle the system gets stuck in Hi-Z mode and will not commence charging. If however the solar panel is disconnected and the reconnected it does commence charging.
Can you please advise whether with the defaulted register settings the system is suitable for such a situation and if so what prerequisites need to be observed?
Thanks Robert