Hi guys,
I have met two SOC issues when doing the charging test of batteries based on BQ27542-G1.
Test Information
Battery rated capacity: 3300mAh
Max Charge current: 1A
The batteries were charged after discharged to 2.9V. There was no current consumption after end of charge.
Battery No. |
Issue |
Test condition |
0 |
The capacity drops from 100% to 98% after end of charge |
Ambient temperature is 40℃, Charge current is 1A, Note: In the charging log, the charge current changes to 0A sometimes due to the temperature protection. |
4,5 |
The charging time from 0% to 1% is very long: BAT4: 1 hour and 49 minutes BAT5: 51 minutes While the normal value is around 20 minutes |
Ambient temperature is 35.5℃, Charge current is 1A Note :This is not the first time to charge the two batteries. In the charge cycles before and after this cycle, the charge times are all OK. |
The attached are the charging log, including the temperature, battery voltage and current and SOC.
The gg file comes from another battery of the same batch of the above batteries .
Can you help to find out the possible reason for such issues?Thank you very much!
Wolf
20210526, BAT0, 40centi degree, 1A charge current.xlsx20210513,BAT4,BAT5,35.5 centi degree.xlsxBY-01.gg.csv