Other Parts Discussed in Thread: UCC2800
Hi,
We intend to use UCC2800 just for its internal overcurrent detection feature. Now, we understand that for this feature to work the design has to ensure that the voltage at CS pin has to exceed 1.5V within the blanking period of 50-150ns. For such a fast detection, during overcurrent the primary of the transformer has to go into saturation to ensure the fault is detected reliably. The question is how do we do this? Our transformer design is such that we are operating with lot of margin from saturation. Hence, during overcurrent conditions we are not able to guarantee that CS pin voltage will exceed 1.5V. What design techniques/suggestions/inputs do you have to enable us to use this feature.
Thanks & Regards,
Priya