This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792EVM: USB2ANY fails to communicate with HID driver. EV2300 works.

Part Number: BQ25792EVM
Other Parts Discussed in Thread: USB2ANY, BQ25792, EV2400, BQSTUDIO, BQ25790

We are evaluating the bq25792 with the EVM. PC is Windows 10. HID device is visible in device manager.  USB2ANY explorer seems to work and sees USB2ANY. Firmware 2.8.2.0.

Communication to the EVM fails. 4 blinks on the LED. Device ACK reported in Battery Studio. BMS also reports "No free adapters are available for use on this system". Since the device is of HID type and virtual com port debugging this error is difficult.

Connected old EV2300 from impedance track days. This does connect to the EVM and registers can be accessed but eventually the interface locks up.

What does it take to get the HID interface to work with Battery Management Studio on this PC?